Skip navigation
TechXchange
Digi-Key TechXchange Communities > Projects and Designs > Discussions
1654 Views 3 Replies Latest reply: Apr 27, 2013 7:59 AM by elutuace RSS
Currently Being Moderated

Apr 17, 2013 8:29 PM

Please help!  I need to choose a Microcontroller

My project entails controling a small motor operated with bluetooth technology,

 

Basically here is the project, when water drips in a small 4 oz tank, some sensors in the tank signals the microcontroller, through bluetooth technology or maybe radio waves, to turn on a small dc motor (the motor is no bigger than the motor that drives those small remote control toy cars), and maybe a solenoid.  Can someone help me out on what all accessories, and parts I need for this project?  I need the motor to turn back and forth like an agitator in a washing machine.  What thing do I need to get this type of motion for a small motor?  Can I control this motion from the microcotroller, I hope so, because I don't want to complicate the matter with gear trains and transmission bundles

  • chaz Novice 2 posts since
    Apr 13, 2013
    Currently Being Moderated
    Apr 19, 2013 10:21 PM (in response to stethius)
    Please help! I need to choose a Microcontroller

    Is the wireless part required? If you are just trying to send an on/off type signal, and the distance is sort, I would suggest IR. You can get an IR diode and detector fairly cheap and it would be fairly easy to use with a microcontroller.  RF will probably require a module, or specilized IC and more code overhead.

     

    From what you described here's what I would do. Use an IR diode to send a signal to the IR detector, which is hooked up to the microcontroller. The level change would trigger an interupt in the microcontroller to start whatever motion of the motor you desire. If you're trying to do both directions with your motor you'd proabably want to use an H-bridge IC. The H-bridge IC would proabably have an up/down input and PWM input, which you can use to control speed and direction with your micocontroller. Look for a H-bridge IC either with integrated FETs and/or an integrated boost converter. Depending on where you plan to get power, there's a good chance you will need a regulator of some sort. I would get a 12V or 24V wall wart, you can use that for your H-bridge, and then regulate it down to 3.3V-5V for whatever microcontroller you plan to use. For microntrollers, I would suggest arduino, or an Atmel microcontroller.

     

    For fun, you could proabably do this without a microcontroller. You could set up some sort of oscilator and a frequency divider (or another oscilator) to set your PWM value and "duty cycle" for the postive and forward movement. You could use an IR reciever hooked to the enable pin of the H-bridge. When the IR reciever is turned on by the IR diode the H-bridge could be enabled with the PWM value. The slower oscilator hooked to the direction input would set when the motor changes directions.

      • elutuace Novice 1 posts since
        Apr 27, 2013
        Currently Being Moderated
        Apr 27, 2013 7:59 AM (in response to stethius)
        Please help! I need to choose a Microcontroller

        I'm going to be using a i2c type of setup, maybe that is something you would want to use as well? the max232 IC should help with greater range as well. Something to consider as most chips have i2c available. Most of the RF band can be quite crowded so unless you really need it to be wireless I would avoid it but that is just me. Here at my house its RF crazyness anything in the 2.4Ghz band I'm hesitant to add, I know there are other bands but that seems to be the most popular as of recently.

         

         

        I'm curious to know the final solution you decide on, I may use a wireless sensor or two if your project demands one and it goes well with yours.

         

        Tom

More Like This

  • Retrieving data ...

Bookmarked By (0)