Skip navigation
TechXchange
Digi-Key TechXchange Communities > Projects and Designs > Discussions
2018 Views 4 Replies Latest reply: Apr 25, 2013 3:21 PM by bobosims RSS
Currently Being Moderated

Apr 11, 2013 8:57 AM

Advice on cleaning out my stereo receiver

Got a stereo receiver that makes these crackling sounds whenever I adjust the volume. Have some spare time this weekend so I was thinking of opening the box up and giving the insides a cleaning. Since this is the first time I’m doing this, does anyone have advice on good electrical contact cleaners and what areas I should focus on to get rid of the annoying sound?

 

Thanks!

  • dolphinboy Novice 2 posts since
    Apr 11, 2013
    Currently Being Moderated
    Apr 11, 2013 12:44 PM (in response to AudioPhile)
    Advice on cleaning out my stereo receiver

    I've had that. Not positive, think I went to Radio Shack for some aerosol stuff. Don't dump on alcohol or other flammable things. Can of compressed air might help, useful to blow out your computer too, but not all that good on a corroded electrical contacts.

  • MetMan Apprentice 86 posts since
    Oct 24, 2011
    Currently Being Moderated
    Apr 11, 2013 1:53 PM (in response to AudioPhile)
    Advice on cleaning out my stereo receiver

    Crackling when you change volume is due to dirty or bad contacts on the volume potentiometer.  I get this from time to time on the sound mixing board I run at our church, and it's easily fixed using spray contact cleaner that is available just for this type of problem.  With the power off, you can spray it directly into the volume pot or slider, move it back and forth, and then power up and see if the crackling is reduced. 

     

    If you try this once or twice and it doesn't improve, then you'll probably have to either try to find a replacment volume potentiometer, or live with the crackling.

     

    Blowing out the dust inside the stereo can help it stay cool, but likely won't help with crackling.

     

    Good luck!

  • Kentrundiga Novice 1 posts since
    Apr 11, 2013
    Currently Being Moderated
    Apr 11, 2013 5:35 PM (in response to AudioPhile)
    Advice on cleaning out my stereo receiver

    Agree with other suggestions here, but would add:  the cleaning supplies that you will find at Radio Shack might do the job, but on older pots the cleaner you use needs a little "body" to continue cleaning and lubricating the wipers.  I would suggest that you find a "control cleaner" that also has silicone - even better you should be able to find a tuner cleaner that has a thick compound that helps keep things "oiled."  Obviously I'm not suggesting OIL, but some cleaning solutions provide a lubricant that really is needed on very dirty or damaged pots.

     

    Kent

  • bobosims Novice 2 posts since
    Apr 25, 2013
    Currently Being Moderated
    Apr 25, 2013 3:21 PM (in response to AudioPhile)
    Advice on cleaning out my stereo receiver

    Consider the line of products from CAIG. I've used these in broadcasting, pro audio, home audio, and hobbyist envrionments with great success. In this case, I'd suggest starting with DeoxIT Gold 100 (if you can apply it in drop format) or DeoxIT Gold GN-5 (if you need to spray to reach the area). Both of those products are safe on older plastics, and not knowing the age of your stereo or what it's made of/with, they would seem to be the safest. While they contain some lubrication, I'd suggest following them (after you've determined that the scratchiness has gone away) with their FaderLube product... it will provide additional lubrication to the moving parts for longer life and best performance. Caig products aren't necessarily cheap, but even their small size containers last quite a while and their products are long-lasting in any application. As someone who does restoration work on old audio gear, those products are my go-to. Good luck!

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points