Skip navigation
TechXchange
Digi-Key TechXchange Communities > General > Discussions
1711 Views 1 Reply Latest reply: Apr 10, 2013 2:10 PM by Mteo2188 RSS
Currently Being Moderated

Apr 9, 2013 1:43 AM

Full Bridge Inverter with MOSFET - IR2110 gate driver

This is the project to make a grid connected inverter.

 

For the full bridge inverter circuit i planned to use IRF2807 (75V Vds, 82A Ids) and Two IR2110 for the driver. I never use IR2110 before and failed many time when i want to make a H-Bridge for DC motor last year.

 

I planned to design the circuit based on this sample project  :

 

111111111111111.jpg

 

 

There are some questions about the schematic since the specification is quiet different.

 

My DC input voltage is 34V (2 series solar panel), The power rating is about 100Watt so the MOSFET should able to drain about 10A max current. The output of the inverter will be connected to 18V - 220V step up transformer. My controller will use hysteresis current control method so the switching frequency is not fixed and varied up to 100kHz.. and i want to isolate (different ground) between my micro controller and power circuit. How can i use the optocoupler to isolate it? is there any optically isolated buffer since i planned to use buffer (micro controller (ATmega 8535, 16MHz -> Buffer IC -> Optocoupler -> IR2110).

 

 

Based on the specification, is there any component that i should change?   read before to change the diode to the fast recovery one, and change the resistor value..

 

If you have to isolate your ground, I would recommend you to use isolation transformer instead of optocoupler. In this, you will no longer need to use high-side capable driver ICs, you will instead use a small gate drive transformer, buffered by the totem-poles.

 

  1111111111111111111111111111111.jpg

 

The transformer is very easy to wind, use small toroid core, about 10mm

outer diameter or even slightly smaller. Make sure that it will not saturate.

 

Just make sure that you follow the polarities, you already know that of course.

More Like This

  • Retrieving data ...

Bookmarked By (0)