Skip navigation
TechXchange
Digi-Key TechXchange Communities > General > Discussions
343 Views 1 Reply Latest reply: Apr 4, 2013 8:33 AM by MikeWeed RSS
Currently Being Moderated

Apr 3, 2013 9:19 PM

I.C.  Help

Im trying to identify this 8 pin ic for weeks now any point in the right direction would be very appriciated .

 

Thanks

Michael Lambert

Image (2).jpg

  • MikeWeed Novice 49 posts since
    Oct 21, 2011
    Currently Being Moderated
    Apr 4, 2013 8:33 AM (in response to mclambert)
    I.C. Help

    It could be a standard dual op amp (LM2904, LMC6482, etc.) being used as a dual comparator. If pin 2 is biased so that it is normally higher than pin 3, then closing the switch will take pins 1,5,6 & 7 high, the collector of the 2N3904 low, thus applying a voltage near ground to the low side of the relay coil. The second op amp is connected as a unity gain amplifier and takes the hi end of the relay coil hi, so the relay and the led turn on.

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points