Skip navigation
TechXchange
Digi-Key TechXchange Communities > General > Discussions
2948 Views 3 Replies Latest reply: Apr 3, 2013 9:06 AM by MikeWeed RSS
Currently Being Moderated

Mar 10, 2013 9:31 AM

Controller for reservoir sluice gate

I  am the engineer for a small HOA that owns/manages a 40 acre lake with 6  sluice gates.  The sluice gates were installed to prevent the  operation/destruction of the flashboard system originally installed to  provide an elevated reservoir level.  I need to find a logic controller  that will receive input from the level sensors and raise the gates a set  amount than wait a set time before raising or lowering the gates.  I am  trying to maintain this reservoir at a level that will not allow more  than 6 inches over the gates.   I can install magnetic reed switch level  sensors in a dampened level container to detect the reservoir level.  I  must keep this system simple.  I was considering a timer switch that  would connect when the level sensor closed and operate the gate actuator  for 60 seconds than wait 5 monutes then if the level sensor was still  closed operate the actuator another 60 seconds than wait 5 minutes.    This system has 2ea 6ft gates with actuators then 4ea 4 ft gates with  one actuator controlling 2 gates.  I would want to operate the 6 ft  gates first then the 2ea 4 ft gates.  I am trying to maintain a balanced  outflow as the gates are installed on each side of the spillway.  Therefore needint 2 controllers. There is 120/240 single phase power at  each site.   Do I need a logic relay or a logic controller?  Where can I  obtain some fast and simple training to program this if needed?   I am a  retired consultant and have an above average computer knowledge, but  also a below average threshold of frustration!!!  

 

I would apreciate any recommendations.  I have wanted to try PLC's for years but do not know where to start.

 

Thanks in advance!

  • WayneT Novice 11 posts since
    Nov 20, 2012
    Currently Being Moderated
    Mar 13, 2013 11:20 AM (in response to damengineer)
    Controller for reservoir sluice gate

    Hello - try taking a look at the 646-1115-ND plc logic controller. Six digital inputs for you to use to monitor your float switches and 4 relay contact outputs to control your sluice gate motors. Though you may need more outputs depending on if the motors for the sluice gates need to be reversed to move the gate in the opposite direction. The controller runs on anything from 100-240VAC single phase and mounts on standard DIN rail.

  • JimHarrison Apprentice 70 posts since
    Sep 9, 2011
    Currently Being Moderated
    Apr 2, 2013 11:37 AM (in response to damengineer)
    Controller for reservoir sluice gate

    You could start with a small computer but I opt for a "Programmable Logic Controller" (PLC) as reccommended above. Figure $300 to $600 for the controller and it may have all the outputs you need

     

    So many to choose from.  Ohmron,Schneider Electric (Modicon), Allen-Bradley, Eator, Siemens, Idec.  Omega has a nice one http://www.omega.com/ppt/pptsc.asp?ref=OCSXL_SERIES.

    • MikeWeed Novice 51 posts since
      Oct 21, 2011
      Currently Being Moderated
      Apr 3, 2013 9:06 AM (in response to JimHarrison)
      Controller for reservoir sluice gate

      While the commercial logic controllers are nice units for the price, few of them have sufficient output current ratings to drive the sluice gate motors, and most of them do not have enough inputs for all the sensors and limit switches. The outputs would have to drive additional contactors or SS relays, meaning additional cost and all the headaches of contact arcing if mechanical contactors are used. These are the reasons I recommended a "homemade" controller that would require more effort but would have a much lower cost.

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points