Skip navigation
TechXchange
Digi-Key TechXchange Communities > General > Discussions
4751 Views 4 Replies Latest reply: Jan 24, 2013 3:29 PM by Elisa_McGuirk RSS
Currently Being Moderated

Jan 10, 2013 4:06 PM

Desoldering

I've been designing some simple circuits in my attempts to learn more, and I think I am ready to start building some small things. I am curious: what do you prefer for desoldering? I'm leaning toward buying some wicking braid, but I wanted some alternate opinions.

  • MetMan Apprentice 88 posts since
    Oct 24, 2011
    Currently Being Moderated
    Jan 11, 2013 4:52 PM (in response to Elisa_McGuirk)
    Desoldering

    I use a desoldering pump most often, but wicking braid is also useful sometimes.  Applying some non-corrosive flux and some extra solder can help with stubborn connections.

  • bluesensual Novice 1 posts since
    Jan 21, 2013
    Currently Being Moderated
    Jan 21, 2013 2:52 AM (in response to Elisa_McGuirk)
    Desoldering

    I've used everything from temp. regulated vacuum desoldering stations to prying resistors off circuit boards with a precision screwdriver while holding a soldering iron under the circuit board.  The former method costly and the latter a little tricky, I would recommend a desoldering device that consists of a hollow soldering tip on a spring loaded plunger.  It plugs in like a soldering iron and allows you to lock the plunger down while you put the tip on the solder joint, melt the solder, push a button on the side of the plunger and , wa la, solder is sucked up into the thing to await its release at your leisure.  When ready to emty  it can  be taken apart and the cylinder cleaned.  A little mineral oil applied to the inside of the cylinder makes for easy future cleaning.

  • Spider99 Novice 7 posts since
    Feb 24, 2012
    Currently Being Moderated
    Jan 23, 2013 4:54 PM (in response to Elisa_McGuirk)
    Desoldering

    Elisa,

    Both solder braid and the desoldering pump are useful where needed. But, to remove multi-leaded components like ICs the only best way is to use Chipquik. Chipquik is so good that if needed you can re-use the IC or component.There is no danger of lifitng a foil trace also. If you need to know how to use it here is a short video. The DigiKey part number is SMD1-ND. The kit will remove many dozens of ICs.

    See the video here ---> http://www.youtube.com/watch?v=7kyaz4Zrd78

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points