Skip navigation
TechXchange
Digi-Key TechXchange Communities > Projects and Designs > Discussions
9283 Views 4 Replies Latest reply: May 10, 2012 1:20 PM by MikeWeed RSS
Currently Being Moderated

May 7, 2012 1:41 PM

Need help providing a variable voltage output 0-10VDC

I'm trying to manage a hydraulic pump using an Arduino microcontroller.  The hydraulic pump is controlled by a Hydraforce 4000165 Proportional valve controller that outputs current to the pump based on a VDC input 0-10VDC.

 

I need a way (or device) that can take a digital signal from the Arduino and convert it to a voltage 0-10VDC to maange the pump controller.  The input resistence of the pump controller is 225Kohm so the device needs to supply up to about 50 mircoamps.

 

This doesn't need to be high frequency (maybe 5 cycle/ second) or many increments of voltage (could probably do with outputting control coltages in 1V steps for at total of 11 steps between (0 and 10V).

 

Any suggestions?

 

Thanks-

  • Mike Novice 8 posts since
    Mar 31, 2011
    Currently Being Moderated
    May 8, 2012 1:31 AM (in response to KC)
    Re: Need help providing a variable voltage output 0-10VDC

    The first thing that comes to mind would be a digital potentiometer. As long as you can provide a 10V source, it should work fine. Based on your requirements, I would suggest about 100k value. Here is a possibility.

    • MikeWeed Novice 51 posts since
      Oct 21, 2011
      Currently Being Moderated
      May 8, 2012 3:10 PM (in response to Mike)
      Re: Need help providing a variable voltage output 0-10VDC

      The source impedance of the digital pot must be much less than the input impedance of

      the controller or else you will lose a significant part of the signal in the source. A 100k

      pot will not work for a load impedance of 225k. A simple fix is to use a rail-to-rail op

      amp connected for unity gain between the pot and controller. I like the LMC6482 for this

      purpose.

      If you don't want to mess with a SPI interface, you might try something like the

      MAX7524. This has an 8 bit input, but you can drive the high 4 bits directly from

      the microprocessor and ground the low 4 bit inputs to get 16 analog voltage steps.

      This chip will probably also require a buffer amp. See the application notes.

        • MikeWeed Novice 51 posts since
          Oct 21, 2011
          Currently Being Moderated
          May 10, 2012 1:20 PM (in response to KC)
          Need help providing a variable voltage output 0-10VDC

          Hi Kevin,

          Yes, I meant MX7524 (or MAX7624). The buffer amp and op amp are the same, shown as "A1"

          in "Typical Operating Circuit" on the MX7524 data sheet. Vref, Vdd and the amp supply

          voltage should all be +10V for your application, and connect -CS and -WR to ground

          to make the output continously follow the digital inputs. You will not need R1 or R2 or

          the 10 pF capacitor,  just connect the op amp output back to Vfeedback on the MX7524.

          Good luck!

          Mike

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points