the micro controller MC 89C51ED2 is installed in high RF Power cabin the problem accour some time it don't work properly to avoid this wat can be the procedure to protect the Micro controller from high RF Power
Grounded Metal shielding
Shielding is the primary solution. Should be a sealed metal enclosure with L/C type feed thrus for the signals and power into and out of the enclosure. Either that or relocate the microcontroller out of the high RF fields...
When you say "Hi Power" how much power are you talking about? I consider 1watt high power
. If you are in the 1 or 2 watt range, I have used a multi-layer board (power and ground plane on the inner layers). Circuit board layout is also important. If your xmtr is mounted or resides on the PC board, make sure the grounds are single point (if they tie together). I also added 470 pf caps (to gnd) on all I/O wires entering or leaving the circuit board. This solved a major RF problem for me and with over a thousand units shipped as of today, there are no problems to report. If you are in the multi-watt range, as the other guys stated, shielding is the way to go.
Rick
thanks to all...
Rf power=40 Watt;
so that we will do this experiment soon the result will be uploaded that shielding , Grounding works or not but on low power its working and on dummy load instead of antenna its also working but with antena its not tested...
Shielding (Faraday cage) is one key aspect, but you also need to consider the power supply and isolating the uP power supply as much as possible from the RF. (Placing the power supply inside the Faraday cage helps, but then you've still got the power feeds to the power supply from "outside".) Note, this is not "just" a ground plane.
You also need to isolate any control lines running into / from the uP to the RF side of the board.
You would expect the system to work with the dummy load and at low power with the antenna (I'm presuming this is what you meant above). The dummy load is absorbing all the energy without transmitting it. And at low power, there's not much energy.
I don't know what frequency you're using, and if your antenna is a patch antenna on the board, or an external antenna. But, an easy solution would be to use an external antenna with the connector through a nice, tightly sealed, grounded metal box holding all your electrical components. (I'd still isolate the RF circuitry, power supplies, and the uP circuitry on the board as much as possible.)
yes frequancy is UHF band...and 50 watt power to transmit note its only its only transmitter contineous power transmission every time when system is on...as soon as my PCBs were final i will give You some practical aspects that what is happening........
How close is the device to the antenna?
About 1.5 meters....
Privacy Statement | Terms & Conditions | Careers | webmaster@digikey.com |
|
701 Brooks Avenue South, Thief River Falls, MN 56701 USA Phone: 1-800-344-4539 or 218-681-6674 or Fax: 218-681-3380 |
|||||||||

Quick Links: