I am desiging a CAN-based networking solution, and I need some help choosing a microcontroller. Price is always a factor. So far I am considering:
Available in several sizes, inexpensive, 8-bit. Requires external CAN transceiver. Can run at 3.3V or 5V.
32-bit ARM Cortex-M0 core. Includes CAN and CANopen drivers in ROM. Also has the CAN transceiver on the chip, so an external one is not required. Needs 3.3V (MCU) and 5V (transceiver).
Are there any other similar parts that I should be considering? Does anyone have any experience with either of these?
#TWiPad
I worked on a few projects that used CAN bus but it was years ago. I beleive we were using a control from Siemens with an external CAN transciever. This paper has some information related to options with Microchip.
I have been very impressed with the power and performance of Silabs products and have used them in several products. I recomend the SDCC compiler which can be used with the free IDE from Silabs and allows full access to all the memory on the chip. The compiler that comes with the dev board only supports a few K and then costs like $5K. SDCC is FREE!
http://www.silabs.com/products/mcu/automotive/Pages/default.aspx
I was not familiar with those. Thanks for the suggestion. Looks similar to the PIC18, but a little more expensive. #TWiPad
Pic18 tops out at 16mips but the silab's parts due up to 100mips. Lots more memory and IO as well. Better off with the PIC18 if you don't need the processing speed / A/D resources / memory. I neaded all 3.
Have you considered the dsPIC30 or 33 series? They run a little more per piece, but have 16-bit architecture and an internal CAN.
I used a PIC24 in a previous CAN project. It has the same architecture as the dsPIC, but without the DSP instructions. The errata on the CAN controller really crippled the usefulness of the chip. I spent a lot of software development time working around the limitations. #TWiPad
Dear Statropy!
I am fan of Fujitsu 16bit CAN controllers and make several designs with it.
Sincerely,
Dmitri Golovatch
Renesas RX62N series is good as well. It has a lot of libaries to get you started in no time.
#TWiPad
We have used AT90CAN128.
This is a good time to look at www.embeddeddeveloper.com. You can pick a supplier or suppliers, choose 8/16 or 16/32 bit core, and specify a CAN port (or multiple ports) and you'll have a nice list.
Privacy Statement | Terms & Conditions | Careers | webmaster@digikey.com |
|
701 Brooks Avenue South, Thief River Falls, MN 56701 USA Phone: 1-800-344-4539 or 218-681-6674 or Fax: 218-681-3380 |
|||||||||

Quick Links: