Skip navigation
TechXchange
Digi-Key TechXchange Communities > General > Discussions
6968 Views 3 Replies Latest reply: Sep 1, 2014 9:09 PM by JohnDavis RSS
Currently Being Moderated

Aug 4, 2014 9:24 PM

Power Supply with Constant Voltage and Current

I have a friend who is a new hobbyist and had a question about power supply he is looking for that I'm not quite sure about as well. He is looking for a power supply that is able to provide 12V with varying Current from 1A to 20A. He also said that the current must remain constant at a certain level, ie. if at 12V 5A, it should remain 5A regardless of load, and this should be the case for all settings for current. The question I have is, is this even possible?

 

From what I know, you can regulate either voltage or current, but not both. Ofcourse I'm no expert, so if there is anything remotely close to what he is looking for, do let me know. Thanks!

  • KISS Novice 5 posts since
    Jul 19, 2011
    Currently Being Moderated
    Aug 13, 2014 8:51 PM (in response to Riley)
    Power Supply with Constant Voltage and Current

    Well in a CC/CV power supply one of the paramters is set as a compliance.

    So, a CC power supply with a compliance of 100V will provide up to 100V to make the constant current.

    With a CV poweer supply, the current is set as a compliance.  e.g, Do not supply more than 10 Amps.

     

    CC is not the same as current limit.  With current limit, you usually lack current regulation.

     

    What he may not know about is an "electronic load".  This device can operate at constant current, constant voltage, constant resistance and constant power.

     

    Another aspect of power supplies is the qudrants of operation.  Most supplies can source a voltage and source or sink a current.

     

    4 quadrant power suppplies or amplifiers can source say a positive voltage and a negative current, so they operate in all 4 quadrants.  V-I+,V-I-, V+I- and V-I+.

    Most supplies operate in the first two.  An electronic load operates in all 4.

  • hsantana Novice 1 posts since
    Aug 28, 2014
    Currently Being Moderated
    Aug 28, 2014 10:43 PM (in response to Riley)
    Re: Power Supply with Constant Voltage and Current

    If you have a constant current then you cannot hold a constant voltage with variations in the load, If, for example, the current is 5A and 12V then the load is V/I=12/5 (2.4) Ohms. If the load changes to 3 Ohms then the voltage must change to R*I=3*5 (15V).

     

    What your friend proposes will not work.

  • JohnDavis Apprentice 53 posts since
    Apr 4, 2014
    Currently Being Moderated
    Sep 1, 2014 9:09 PM (in response to Riley)
    Power Supply with Constant Voltage and Current

    simply put, you cannot have both things constant because they affect each other based on the load resistance. As one changes, the other changes as well, you can only keep one of them constant, while the others in a certain range.

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points