Skip navigation
TechXchange
Digi-Key TechXchange Communities > Component Discussion and Reviews > Discussions
5784 Views 1 Reply Latest reply: May 7, 2014 1:25 PM by davecuthbert RSS
Currently Being Moderated

May 7, 2014 9:57 AM

Amplify High Frequency Signal

I'm trying to do something a little outside of my normal sphere of interests.  I've got a high frequency signal, 30Mhz, that I'm trying to amplify.  If possible, I'd like to bump it up about tenfold, from the 1-2 volt range to the 10-20 volt range.  If I remember correctly, for voltage, an increase of 20dB is the same as 10x. 

 

Are there amplifiers out there that could handle this?  I'm assuming that I won't have to make something out of discrete components.  If so, where would I start looking to figure it out?

 

Thanks for your help!

  • davecuthbert Journeyman 65 posts since
    Feb 18, 2014
    Currently Being Moderated
    May 7, 2014 1:25 PM (in response to LanceLK)
    Re: Amplify High Frequency Signal

    Assuming you mean 20 volts P-P, a 1 watt RF amp will do the job. Your amp needs these specs:

     

    30 MHz +/-

    Gain >20 dB

    Power > 30 dBm

     

    Mini-circuits stocks these and the ZHL-1-2W is suitable covering 5-500 MHz with a gain of 29 dB and a maximum output power of 33 dBm. The prices is $475.

     

    Of course you can build your own amplifier at this power level.

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points