Skip navigation
TechXchange
Digi-Key TechXchange Communities > General > Discussions
15137 Views 3 Replies Latest reply: Apr 25, 2014 12:34 AM by NITMOI RSS
Currently Being Moderated

Apr 21, 2014 10:26 AM

Capacitor and inductor - voltage and current changes

I've looked on the internet but haven't really read anything that intuitively explains why the voltage across a capacitor and the current through an inductor can't change instantaneously.  Can anybody explain it so that I can easily understand what is going on?

  • LanceLK Novice 42 posts since
    Apr 4, 2014
    Currently Being Moderated
    Apr 23, 2014 11:58 AM (in response to Riley)
    Capacitor and inductor - voltage and current changes

    Hey Riley, the math explanation is actually pretty straightforward even if you don't know basic calculus. 

     

    The current through a capacitor is given as the capacitance times the change of the voltage versus time.  So, the faster the voltage changes, the greater the current.  Also, the greater the current, the greater the voltage change.  If the voltage were to change instantly, that would mean that the current would be extremely large - infinitely large.

     

    The opposite for the inductor.  The voltage across an inductor is given by the inductance times the change in the current versus time.  So, the faster the current changes, the greater the voltage.  If the current were to change instantly, the voltage would be infinitely large.

     

    Hopefully this helps you understand the limitations more intuitively, at least from a mathematical perspective. 

  • NITMOI Novice 10 posts since
    Mar 14, 2014
    Currently Being Moderated
    Apr 25, 2014 12:34 AM (in response to Riley)
    Capacitor and inductor - voltage and current changes

    For those old enough to have worked on cars with points, that's how the coil is able to generate 1000's volts for the spark plug.  The points open up (very fast) and the coil 'must keep the circuit connected' thus raising the voltage until the spark plug literally ionizes the gas in the cylinder thus completing the circuit.

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points