Skip navigation
TechXchange
Digi-Key TechXchange Communities > Component Discussion and Reviews > Discussions
10352 Views 3 Replies Latest reply: Apr 24, 2014 1:19 PM by davecuthbert RSS
Currently Being Moderated

Apr 22, 2014 11:27 AM

High voltage, low current fuse

I'm looking to use a device that would function as a fuse. However, I need a device that can withstand high voltage (~5 kV), but to limit the current to ~40 mA. I've found fuses that can limit in the mA range, however the max voltage is in the V range. I've also found high voltage fuses, however they limit in the A range. Does anyone know of anything that would work for my specifications? Thanks!

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points