Skip navigation
TechXchange
Digi-Key TechXchange Communities > Component Discussion and Reviews > Discussions
6826 Views 3 Replies Latest reply: Apr 16, 2014 7:45 AM by jhanlon_ysi RSS
Currently Being Moderated

Apr 15, 2014 3:07 PM

RM-W Series

Subtitle: 

Cable Clamps for RM-W Series Circular Connectors

Supplier: 

Hirose Electric Co Ltd

Description: 

Please limit comments in this discussion to this series.

  • jhanlon_ysi Novice 2 posts since
    Feb 24, 2014
    Currently Being Moderated
    Apr 15, 2014 3:07 PM (in response to Online Catalog)
    RM-W Series

    It would be nice to know what range of cable sizes each clamp supports.  Cables are available in many sizes between 4mm, 5mm, 6mm, 7mm, etc.  I have a 4.5mm cable.  Do I assume that the 4mm size can clamp "down-to" 4mm, and thus accepts anything from 5mm down to 4mm?  Or do I assume that 4mm is a hard limit, and it cannot support a larger diameter cable?

    • Adam Apprentice 40 posts since
      Apr 1, 2011
      Currently Being Moderated
      Apr 15, 2014 3:50 PM (in response to jhanlon_ysi)
      RM-W Series

      It looks like it would be a hard limit (with a tolerance) based on their spec table and note listed on their datasheet for the majority of their clamps. If they were able to accept a range they should list it in the datasheet.

       

      Example: RM21WTP-CP(8)(71)

       

      • jhanlon_ysi Novice 2 posts since
        Feb 24, 2014
        Currently Being Moderated
        Apr 16, 2014 7:45 AM (in response to Adam)
        Re: RM-W Series

        Agreed.  I didn't think to check the other cable clamps in the datasheet.  This sounds like a safe assumption since the construction of the RM12-WBP-CP version appears to be of the same style of construction.

         

        I will add that for the RM12-WBP-CPs clamps they quote both the A-diameter of the grommet ID and a cable diameter, and they quote a single A-diameter for two different cable diameters, twice (see image below).

         

        RM12.JPG

         

        This led me to assume that each clamp was designed to clamp "down-to" the cable diameter listed, but would allow a cable with a diameter as high as the A-diameter.  But that assumption would allow elimination of the 5mm and 7mm versions, so it's not a good assumption!!!

         

        So, now I think I will just look for cables that meet the recommended cable diameters of 4mm, 5mm, 6mm, or 7mm, +/-.2mm.

More Like This

  • Retrieving data ...

Bookmarked By (0)