Skip navigation
TechXchange
Digi-Key TechXchange Communities > Component Discussion and Reviews > Discussions
20387 Views 7 Replies Latest reply: Mar 8, 2014 9:56 AM by davecuthbert RSS
Currently Being Moderated

Nov 23, 2013 9:44 PM

Zener diode size vs wattage?

Hello all. I'm repairing a circuit board from a Crate PA6FX mixer amp, and it has some scorched zener diodes with a very clear part number 1N5353B. This comes up as a 5 watt, 16v diode. There is an additional number below this on the diode, 1061; I haven't found that to match any part numbers or mean anything relevant to the part's rating.

When they arrived, the new diodes look similar; black body with silver markings, but the body of the new diodes are at least 30% smaller than the diodes that are in place. I looked under the part number listings again to see if I had perhaps picked the wrong wattage rating, but none of the diodes under that part number have a different wattage rating or different physical size. Has diode composition improved that much in the past 10-15 years or so? Am I missing something?
Thank you in advance for any insight you can offer.

MJ

  • WayneT Novice 12 posts since
    Nov 20, 2012
    Currently Being Moderated
    Mar 3, 2014 3:42 PM (in response to putergurl)
    Zener diode size vs wattage?

    The additional 4 suffixes marked on the part would be for Date/Lot Code information. Also, this part is offered in several through hole packages. The part number does not call out a specific package case size. The case sizes I see offered for this part are 5w. So as long as the dimension will work for the application I see no reason why you can't use another case size.

  • davecuthbert Journeyman 65 posts since
    Feb 18, 2014
    Currently Being Moderated
    Mar 6, 2014 9:59 AM (in response to putergurl)
    Re: Zener diode size vs wattage?

    The relatively small 1N5353B zener diode achieves its specified 5 watt rating by heatsinking through the leads. The datasheet specifies 3/8" leads to an infinite heatsink. This cannot be easily achieved in practice and so the practical rating is much less than 5 watts.

     

    I've used two "tricks" to cool off these types of zener diodes. One is to use the entire lead length as a heatsink. To shorten the linear length each lead is formed into a spiral around a drill bit. The other is to cut a copper penny in half and solder it to the lead right at the diode body.

     

    I once saw a design in which the engineer ran 5 watt diodes at 5 watts. Being mounted on the underside of the PCB they would melt the solder and fall out. The engineer's fix was to slather the PCB with epoxy to hold the diodes in! That is not a good design.

    • davecuthbert Journeyman 65 posts since
      Feb 18, 2014
      Currently Being Moderated
      Mar 6, 2014 7:50 PM (in response to putergurl)
      Re: Zener diode size vs wattage?

      That's a good point so let's work the numbers. The datasheet specs are at DC and the inductance effect is of course at AC, but there there's enough data to ball park it.

       

      The Microsemi datasheet shows that at 75 mA a 16 volt 1N5453 has a dynamic impedance of 2.5 ohms. Using a total length of 2" and the rule-of-thumb of 20 nH/inch the zener has an inductance of 40 nH. We'll ignore the zener capacitance for now. At what frequency is the inductve reactance equal to the dynamic impedance? That's 40 nH and 2.5 ohms and the frequency is 10 MHz. So, unless the zener is being used without a shunt capacitor above 10 MHz the lead inductance is not an issue.

       

      As to the zener capacitance, to have a reactance of 2.5 ohms at 10 MHz it would have to be 6 nF. I recall measuring a 1N5353 many years ago - I forget what breakdown voltage it was - and the capacitance was less than 1 nF. So, I think we can ignore the capacitance for this exercise.

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points