About Scheme-it

Current Version:

The current Scheme-it version is 2.4

Version 2.4

This version adds the ability to embed schematics into blogs, TechXchange articles or web pages.

Version 2.3

The major feature in this version is the multi-page capability. Users may now have up to 8 schematic pages. Pages can be given a custom name with up to 15 characters. Additional changes include new schematic symbols, new search capabilities, and many internal code improvements.

Version 2.2

This release adds schematic sharing and new schematic symbols, along with bug fixes.

Version 2.1

Bug fix release. Also updated the version number to match the internal number. The previous 1.1 release was in fact 2.0 so the notes have been updated to reflect this.

Version 2.0

A fairly significant release that reworked the internals of the application. The rework resolved a range of internal issues, and added some new features. The rework also provided an improved architecture that will facilitate future updates and enhancements.

Versions 0.1 to 2.0

The original versions of Scheme-it. These released included a number of bug fix and feature enhancements, along with addition of new symbols.