ProcureMinute

Got a minute? Learn more about what Digi-Key has to offer for your procurement needs.

Contact Us

Send questions about site content and general comments to purchasingpro@digikey.com.

Chipmakers closed 49 wafer fabs between 2009 and 2011

Forty-three percent of the closed fabs used 150 mm wafers

02/17/2012

Chipmakers build more 300mm fabs
Chipmakers are building more 300 mm wafer fabs as they close older facilities that use small size wafers.
Semiconductor companies closed 49 wafer fabs from 2009-2011, but wafer capacity increased because more 300 mm wafer fabs came on line, according to researcher IC Insights.

The industry has been reducing its older capacity since 2007. The bulk of these closings were older capacity includes fabs that use 200 mm, 150 mm, 125 mm and 100 mm wafers, the Scottsdale, Ariz.-based researcher reported.

The decline in 200 mm and smaller capacity continued through 2010 and 2011 as suppliers closed or upgraded fabs that used smaller wafers in order to produce integrated circuits on more cost-effectively larger wafers. A few of the fabs are being refurbished to handle large wafers or production of discrete semiconductors.

More semiconductor manufacturers are expected to shutter older fabs as they transition to the “fab-lite” business model or become completely fabless, according to IC Insights.

Forty-three percent of the fabs closed from 2009 to 2011 were 150 mm wafer fabs, while 13 were 200 mm; 7 were 125 mm; 5 were 300 mm; and 3 were 100 mm. One of the 300 mm fabs that ceased operation was owned by Qimonda, which went out of business in early 2009, IC Insights noted.

Regionally, Japan and North America each had 17 wafer fab closures, followed by Europe with 12 and South Korea with 3. One of the wafer fab closures in Japan was a 300 mm IC fab operated by Sony. However, the fab is being retrofitted and will return to service to produce image sensors for the company.

The Qimonda wafer fab in Sandston, Va., was the only 300 mm wafer fab closed in North America during this time. Three 100 mm wafer fabs were closed in the three-year span. These included fabs owned by DALSA in Bromont, Ontario, Canada; ON Semiconductor in Slovak Republic; and Diodes in England.

Brian Matas, vice president research at IC Insights, said that although older fabs have closed there has been a net gain in overall semiconductor capacity. More 300 mm fabs came on line, which more than make up for the capacity loss of the closing of the older fabs.

He added that the amount of installed IC wafer capacity increased 6 percent in 2010 and another 8 percent in 2011 as the number of 300 mm wafer fabs increased during those years. In 2010, there were 73 300 mm wafer fabs on line, compared to 68 in 2009. In 2011, the number of 300 mm facilities increased to 79.

“The fabs are going off-line are doing so mostly because the bigger fabs are coming on line. In some cases semiconductor companies are upgrading facilities or operations to more efficient operations and bigger wafer sizes,” said Matas.

 

All parts by: Title Manufacturer Category Manufacturer Part No.   |   Electronic parts by: Component Title Manufacturer Category Manufacturer Part No.
Part categories by: Name Manufacturer   |   Manufacturers by: Name Number of Parts   |   Products by: Category Title   |   Grouped parts by: Title Model Number
Austria Parts  Canada Parts  France Parts  Germany Parts  Italy Parts  Japan Parts  Spain Parts  United Kingdom Parts United States Parts