Back to top

Apex Microtechnology

- Apex Microtechnology develops and manufactures precision power analog monolithic, hybrid and open frame components for a wide range of industrial, test and measurement, medical, aerospace and defense applications. These devices are typically used to generate motion control, such as driving piezo electrical devices, and brush and brushless DC motors. With more than 300 catalog “off-the-shelf” products, Apex Microtechnology is a recognized leader for consistently developing products that lead the industry in terms of performance, quality, and reliability. Founded in 1980, Apex Microtechnology was acquired in 2007 by Cirrus Logic, a premier supplier of mixed-signal processing components for audio and energy markets. Following a five-year tenure as a division of the Austin, Texas, based developer of complex chip designs, Apex Microtechnology has returned to a stand-alone, privately-held corporation with its sale to a private investor group. The company is headquartered in Tucson, Ariz., USA.

Newest Products View All (13)

Image of  Apex PA13EEA Power Operational Amplifier

PA13EEA Power Operational Amplifier

Apex Microtechnology’s PA13EEA is a 15 A, 90 V power operational amplifier with low thermal resistance (1.1°C/W). Target applications include driving resistive, inductive, and capacitive loads such as motors, magnetic deflection, transducers, and programmable power supplies.

Learn More
MP118FD Bandwidth Amplifier

MP118FD Bandwidth Amplifier

The MP118FD is a low cost, low quiescent current power operational amplifier that integrates several new layers of onboard circuit protection

Learn More
Image of Apex Microtechnology's PA92 High-Voltage Power Operational Amplifiers

PA92 High-Voltage Power Operational Amplifiers

The PA92 high-voltage, low quiescent-current MOSFET op amp is designed as a low-cost solution for driving continuous output and pulse currents.

Learn More
Image of Apex Microtechnology's PA12 and PA12A Power Operational Amplifier

PA12 and PA12A Power Operational Amplifier

The PA12 high-voltage, very-high-output current op amp is designed to drive resistive, inductive, and capacitive loads.

Learn More
Image of Apex Microtechnology's SA01 Pulse-Width Modulation Amplifier

SA01 Pulse-Width Modulation Amplifier

The SA01 amplifier can supply 2 KW to the load and features a single supply operation, 10 A continuous output, and hermetic package.

Learn More
Image of Apex Microtechnology's PA03 Power Operational Amplifiers

PA03 Power Operational Amplifiers

PA03 power op amps feature MO-127 copper power dip package, high internal power dissipation to 500 W, and internal SOA protection.

Learn More

Product Training Modules View All (1)

Power Analog Portfolio

Power Analog Portfolio

Duration: 10 minutes

Providing complex circuit designs in a single package, enabling high density designs with a reduced time to market.

Featured Videos View All (3)

Apex Microtechnology DB64 SA306-IHZ Demonstration Board

DB64 SA306-IHZ Demonstration Board

Apex Microtechnology- SA306-DB64

Apex Microtechnology - SA306-DB64

Apex Microtechnology - Techniques for Power Amplifier Stability

Techniques for Power Amplifier Stability - Learn 3 different techinques to address ''stability'' issues in an electrical system when designing with high power amplifiers