RoHS Recast Still Causes Confusion in the Supply Chain

Many in the supply chain have questions about what falls under the scope of the revised RoHs, the European law that restricts the use of lead and other substances in electronics equipment.

By Gina Roos

Image of RoHS Recast still causes confusion in the supply chainMost electronics OEMs understand that they must meet new requirements of RoHS Recast, an update of the European Union's (EU) Restriction on the Use of Certain Hazardous Substances (RoHS) Directive. RoHS, which went into effect in 2006, was revised last year, and there is some confusion in the electronics industry over several key points of the law.

Design Chain Associates (DCA) recently addressed some of the most frequently asked questions about changes to the law which restricts the use of lead, mercury, cadmium, hexavalent chromium, polybrominated diphenyl ether, and polybrominated biphenyl in electronics equipment.

While no new substances were added to the list, the revised RoHS made changes in the scope of the law. Revisions to the law also impact CE marking, exemptions, data collection, and risk management.

Ken Stanvick, DCA's senior vice president said one of the biggest changes concerns the scope of the law. Medical devices (Category 8) and industrial monitoring (Category 9) will come into the scope of the law in 2014. All other electronics and electrical equipment not covered in other categories of equipment will come into scope in 2019.

Military and aerospace products, along with several other types of equipment including large-scale stationary tools, large-scale fixed installations and implantable medical devices, remain out-of-scope.

Stanvick added that there has been some confusion about whether subassemblies fall into scope of RoHs. When subassemblies are incorporated into a finished product, if the finished product is in scope, the subassemblies must also be RoHS compliant.

Similarly, components are not in scope under RoHS, but they do become impacted by it based on the finished product application.

Also, evaluation boards, reference designs and kits used by engineers to evaluate semiconductor chips are not in scope with the directive. User guides are also not under the scope of the law. However, pouches and carrying cases used with the equipment have to comply with RoHS, Stanvick said.

There also appears to be some questions around the role of contract manufacturers. A contract manufacturer is not considered to be a finished product manufacturer unless they place their name on the product.

Questions have been raised around the connection between the EU's Registration, Evaluation, Authorization, and Restriction of Chemical substances (REACH) regulation and RoHS Recast. Stanvick noted that there is an effort to make sure they complement each other.

An example cited is the precautionary principle in which four substances have been identified as substances of very high concern (SVHC) under REACH. Although no new substances have been banned under revised RoHs, the four SVHCs will likely be the first ones evaluated under the RoHS Recast as possible additions to the list of banned substances, according to Stanvick.

The SVHC substances include:

  • Hexabromocyclododecane (HBCDD): a brominated flame retardant used as packaging material, video cassette recorder housing, and electric and electronic equipment
  • Bis (2-ethylhexyl) phthalate (DEHP): a plasticizer used in the manufacture of articles made of PVC and as a dielectric fluid in capacitors
  • Benzylbutylphthalate (BBzP), also called benzyl butyl phthalate (BBP): a phthalatetrade (Palatinol BB, Unimoll BB, Sicol 160, or Santicizer 160) used as a plasticizer in manufacturing of articles made of PVC
  • Dibutylphthalate (DBP): a plasticizer used in manufacturing of articles made of PVC and as an additive to adhesives or printing inks
However, there is nothing in the RoHS Directive that states a finished product must be compliant to REACH.
Only one CE mark needed

Image of Ken Stanvick, senior vice president of Design Chain Associates
Medical devices and industrial monitoring will come into the scope of RoHS in 2014, said Ken Stanvick, senior vice president of Design Chain Associates.
The recast also includes a CE mark requirement. This provides a formal set of requirements for manufacturers to demonstrate RoHS compliance, making the CE mark universally accepted across the European Union. Currently, there is a mix of different marks created in the industry, ranging from special symbols to logos to signify RoHS compliance, which will no longer be sufficient.

"This will always be an issue," said Stanvick. "There is no ideal answer. There have been many methods used including different part numbers, special symbols, and date codes to identify compliance status with mixed results."

This does not mean more than one CE mark is required on a product. Having one is sufficient, said Stanvick. If a product already has a CE mark to indicate that it is compliant under another directive, such as the Machinery Directive or the Low Voltage Directive, product manufacturers do not need to add one for RoHS. Instead, manufacturers will be required to update the declaration of conformity (DoC) and technical documentation to reflect RoHS compliance.

In addition, CE marking does not pertain to components, only finished product, which includes both consumer and commercial goods.

Time limits for exemptions

Exemptions now have time limits by category type and companies must submit renewal applications 18 months before the exemption expires. Under the RoHS Recast, in general, exemptions for Categories 1-7, 10, and 11 are valid for up to five years, and up to seven years for Categories 8 and 9.

There is no restriction on who can ask for exemptions. Just about any organization can request an exemption including product manufacturers, authorized manufacturer representatives, industry associations, NGOs, consultants, and lobbyists.

One question that continues to be asked pertains to the lead (Pb) exemption in ceramic capacitors. The exemption for lead in the dielectric ceramic in capacitors for a rated voltage of less than 125 Vac or 250 Vdc expires on January 1, 2013. After that date, those capacitors may be used in spare parts for EEE placed on the market before January 1, 2013, explained Stanvick.

He said "almost without exception, the manufacturers of ceramic capacitors have already reformulated their products to comply."

Stanvick recommends companies ask for full materials composition disclosure and keep it current as a way to prove RoHS compliance and to manage any changes. He said the following must be included in a technical documentation file for RoHS:

  • A general description of the product
  • Conceptual design and manufacturing drawings and schemes of components, sub-assemblies, circuits, etc.
  • Descriptions and explanations necessary for the understanding of those drawings and schemes and the operation of the product
  • A list of the harmonized standards and/or other relevant technical specifications the references of which have been published in the Official Journal of the European Union, applied in full or in part, and descriptions of the solutions adopted to meet the essential requirements of the legislative instrument where those harmonized standards have not been applied. In the event of partly applied harmonized standards, the technical documentation shall specify the parts which have been applied
  • Results of design calculations made, examinations carried out, etc.
  • Test reports

Manufacturers have to demonstrate that the product is designed to be compliant by documenting disclosure and content information, and that they have a quality system in place to maintain the quality or performance of that product relative to the RoHS Directive, said Stanvick.

Some companies are asking if ISO 9001 is an approved way to show compliance. The directive only expects that a manufacturer has a quality system in place, but does not require any specific system.

Managing risk

Stanvick noted that if a manufacturer or supplier only provides a certificate of compliance (C of C) for their RoHS-compliant product, supply chain professionals need to review the risks and options. They should ask whether the supplier is a “single source” and if the supplier has a plan to provide additional information.

Should a company test incoming parts with an XRF analyzer? Stanvick does not recommend testing incoming parts, whether with an XRF analyzer or sending it out to a third-party test lab. "It's about process control, knowing who you're buying from, having good controls in place with a particular supplier, and having good documentation trails," he said. "Testing is costly."

To manage risk, Stanvick recommends developing a formal specification, documenting what is required to substantiate a claim of RoHS compliance by suppliers. He also said to make sure that compliance to this specification is referenced in the purchasing agreement and enforced.

A third recommendation is to organize suppliers and their products according to their level of risk and take appropriate action to validate their data or replace them.

Tier 1 suppliers are low risk, so manufacturers can accept information as provided by the supplier. For Tier 2, or medium risk suppliers, Stanvick recommends that the information be reviewed and approved by the compliance engineer. Internal audit results may be required or requested.

For Tier 3, or high-risk suppliers, information must be certified by a test lab or independent third-party auditor. "Have a plan to remove that supplier from your process," Stanvick added.

Although there are not any rules in place in terms of how all documentation must be delivered or stored, Stanvick said it is reasonable to assume that storing it electronically is appropriate due to the volume of data. The DoC and the technical file must be kept on file for ten years and available to the national enforcement authorities.

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of Digi-Key Electronics or official policies of Digi-Key Electronics.