Thermal Products

Devices that are used to provide cooling to electrical and electronic components.

DC Fans DC Fans Cooling devices that are designed to produce a flow of air out of one side or end of the unit. The devices in this family are designed to be used with a direct current.
View all DC Fans
AC Fans AC Fans Cooling devices that are designed to produce a flow of air out of one side or end of the unit. The devices in this family are designed to be used with an alternating current.
View all AC Fans
Finger Guards and Filters Finger Guards and Filters Devices that are designed to prevent items from accidentally entering or exiting a fan.
View all Finger Guards and Filters
Heat Sinks Heat Sinks Cooling devices that work by absorbing heat from an object and then dissipating that heat into the surrounding air.
View all Heat Sinks
Pads, Sheets Pads, Sheets Devices that are designed to secure and/or provide for enhanced thermal transfer between heat sinks and components. The items in this family are in the form of a thin, cuttable, rectangular, flexible sheets. Some of these items may be precut to fit on predefined component sizes.
View all Pads, Sheets
Adhesives, Epoxies, Greases, Pastes Adhesives, Epoxies, Greases, Pastes Devices that are designed to secure and/or provide for enhanced thermal transfer between heat sinks and components. The items in this family are in a spreadable semi-liquid state.
View all Adhesives, Epoxies, Greases, Pastes
Thermoelectric, Peltier Assemblies Thermoelectric, Peltier Assemblies Devices that are designed for thermal transfer using the Peltier effect (as current passes through the junction of two different metals or semiconductors, heat is produced on one side of the junction and absorbed on the other side). The items in this family will contain a Peltier module, heat sinks and may also contain a fan.
View all Thermoelectric, Peltier Assemblies
Thermoelectric, Peltier Modules Thermoelectric, Peltier Modules Devices that are designed for thermal transfer using the Peltier effect (as current passes through the junction of two different metals or semiconductors, heat is produced on one side of the junction and absorbed on the other side).
View all Thermoelectric, Peltier Modules
Accessories, Kits Accessories, Kits Supplementary items used with thermal products.
View all Accessories, Kits