MOSFET, Bridge Drivers - External Switch
A semiconductor device that is designed to interface between power signals and an external MOSFET or Bridge architecture circuit.
MOSFET, Bridge Drivers - Internal Switch
A semiconductor device that is designed to interface between power signals and an internal MOSFET or Bridge architecture circuit.
Display Drivers
Semiconductor device that is designed as an interface between a display and the rest of the circuit, providing the drive signals for the display.
Hot Swap
Semiconductor device that provides the protection needed to allow other components to be inserted or removed from a circuit while there is power live in the circuit.
Laser Drivers
Semiconductor device that is designed as an interface between a laser and the rest of the circuit, providing the drive signals for the laser.