Isolators, Optoisolators, Photocouplers

Devices that are used to electronically separate circuits but still allow for signals to be transferred between the circuits.

Transistor, Photovoltaic Output Transistor, Photovoltaic Output Devices that are used to electronically separate circuits but still allow for signals to be optically transferred between two circuits. Components in this family use a transistor on the output of the device.
View all Transistor, Photovoltaic Output
Logic Output Logic Output Devices that are used to electronically separate circuits but still allow for signals to be optically transferred between two circuits. Components in this family use some form of a logic gate circuitry on the output of the device.
View all Logic Output
Digital Digital Devices that are used to electronically separate circuits but still allow for digital signals to be transferred between the circuits.
View all Digital
Triac, SCR Output Triac, SCR Output Devices that are used to electronically separate circuits but still allow for signals to be optically transferred between two circuits. Components in this family use a TRIAC or SCR on the output of the device.
View all Triac, SCR Output
Special Purpose Special Purpose Devices that are used to electronically separate circuits but still allow for signals to be transferred between two circuits. Components in this family use some special circuitry on the output of the device.
View all Special Purpose