Discrete Semiconductors

Devices that contain an individual circuit and provide a single function. These devices are built with materials that have an electrical conductivity that falls between the conductivity of a conductor and an insulator.

Diodes, Rectifiers Diodes, Rectifiers Semiconductor devices that are designed to allow current flow only in one direction.
View all Diodes, Rectifiers
Thyristors Thyristors Semi conductive devices with three pn junctions (4 layers).
View all Thyristors
Transistors, FETs, IGBTs Transistors, FETs, IGBTs Semiconductor devices that contain more than one pn junction or channel and are often used to amplify or switch signals.
View all Transistors, FETs, IGBTs
Variable Capacitance, Varicaps, Varactors Variable Capacitance, Varicaps, Varactors A semiconductor device with two terminals that has a capacitance which will vary with the amount of voltage applied across the terminals.
View all Variable Capacitance, Varicaps, Varactors
Kits Kits Groupings of discrete semiconductors.
View all Kits