Devices that are designed to keep electrical devices safe from excess voltage and/or current.
Fuses, Circuit Breakers, Inrush Current Limiters
Devices that are designed to keep components safe in situations where an excessive amount of current is suddenly introduced to a circuit.
TVS (Transient Voltage Suppression)
Devices that are designed to keep components safe in situations where there is a sudden excessive amount of voltage introduced to a circuit.
Thermal Cutoffs, Cutouts
Devices that are designed to keep components safe in situations where there is an excessive amount of temperature. Component in this family will open the circuit they are installed in when the functioning temperature of the device is exceeded.
Temperature Regulators, Switches
Devices that are designed to keep components safe in situations where there is an excessive amount of temperature. Component in this family will open or close a circuit that they are installed in when the switching temperature of the device is exceeded.
Surge Protection IC's
Devices that are designed to keep electrical devices safe from excess voltage and/or current. Components in this family are designed using semiconductor materials.
GFCI (Ground Fault Circuit Interrupter)
These devices are designed to allow for a stoppage of current flow when the device detects a discrepancy between the current flow in the neutral and hot lines of a circuit.
Lighting Protection
Devices that are specifically designed to protect LED and other lighting circuits in situations where there may excessive current, voltages, reverse connections and more.