Devices of the same style that most often mate with another device of the same style but opposite gender in order to transfer signals or power from one area of a device to another.
Rectangular Connectors
Interconnect devices that have a specific shape and design. The items in this category will have a rectangular look to the mating end of the device.
D-Sub, D-Shaped Connectors
Interconnect devices that have a specific shape and design. The items in this category will have a "D" look to the mating end of the device.
Circular Connectors
Interconnect devices that have a specific shape and design. The items in this category will have a circle shape on the mating end of the device.
Modular Connectors
Interconnect devices that have a specific shape and design. The items in this category were originally designed to be used in telecom device.
Barrel
Interconnect devices that have a specific shape and design. The items in this category will either have a cylindrical shape or are able to mate with a device with a cylindrical shape. These types of devices are most often used with audio or direct current power equipment.
Banana and Tip
Interconnect devices that have a specific shape and design. The male gendered items in this category will either have a cylindrical shape composed of spring like metal strips or a smaller version of the device without the spring like strips.
Backplane Connectors
Devices that usually connect two boards together, one of the boards containing multiple connectors aligned parallel to each other. This board is usually mounted in a rack or case.
Flat Flexible (FFC, FPC) Connectors
Interconnect devices that have been designed to work with a specific cable type. The items in this category will work with cables composed of flattened conductors placed parallel to each other and molded over.
Between Series Adapters
Devices used to convert from one connector style to another. Each end of these devices will contain a different style of connector.
Blade Type Power
Interconnect devices that have been designed to work with larger power requirements. The male gendered items in this category will have contacts that have a blade style.
Fiber Optics Connectors
Interconnect devices that have been designed to work with a specific cable type. The items in this category will work with cables composed of a glass or plastic thread within a jacketed material.